Can Power Meter Configuration Utility (PMCU) read on-board logs on a CM2000 via a Link150
Issue
ION Setup cannot read on-board logs for a CM2000 when communicating via a Link150 (Ethernet gateway). Power Meter Configuration Utility (PMCU) cannot communicate to a CM2000 that's downstream of a Link150.
Product Line CM2000
Link150
PMCU
ION Setup
PME 8
Environment Installation/Setup
Cause
Power Monitoring Expert (PME) and ION Setup can communicate with the CM2000 downstream a Link150, but ION Setup is not able to read on-board logs.
Resolution
When trying to retreive on-board logs, PMCU can be used to communicate to the CM2000 serially and downstream of an EGX100/300.
However, when the CM2000 is downstream of a Link150 ethernet gateway, PME is the only software that allows the user to view the on-board logs.
Sign up for all the latest solutions, offers and best practices straight to your inbox.
All done!
Thank you for subscribing to updates from Schneider Electric.
We are excited that you have joined the group. You will receive your welcome email soon describing the program and what to expect in the upcoming weeks. Enjoy!