Technical FAQs

Ask a Question

Osisense XC - Does the association ZCKJ5 + ZCKE09 operate properly?

The association ZCKJ5 body (slow break contacts) + ZCKE09 head (snap action mechanism) or ZCKE095 or ZCKE096, does not operate properly because the ZCKE09* head has a short stroke, compatible with a snap action contact block. That's the reason why, in the Osisense XC catalogue, there is an information about the ZCKJ bodies compatibility (snap action contacts only) : ZCKJ1, ZCKJ2, ZCKJD31, ZCKJD39.

Was this helpful?
What can we do to improve the information ?