Browse FAQs

Preventa XCS - Technical description of the XCSM4102L10TQ safety switch

Published date: 07 June 2019

The adapted reference XCSM4102L10TQ is a standard product XCSM4102L5 with a cable length of 10m instead of 5m + bulk packaging of 10 pieces (TQ). This reference is not shown into the Preventa XCS catalogue. It is available to order without marketing restriction. Attached for information the XCSM4102L5 data sheet


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.