Browse FAQs

What is the definition for the SoMachine memory area when building an application?

Published date: 16 August 2019

Below is the definition for each memory area (0-5) when compiling your SoMachine application.

Area 0 = %MW
Area 1= %I
Area 2=%Q
Area 3= Retain
Area 4= Application size + local variables
Area 5 = Persistent variables
If you defining local variables without an address and persistence,  than memory area 4 will tell you how much memory is available for the application and local variables.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.