Technical FAQs

Ask a Question

Preventa XCS - Dimensions of the obsolete XCSPL5/7 having 5 digits in the part number, discontinued in 2000

Hereafter the dimensions (in mm) of the obsolete XCSPL5/7 switch having 5 digits in the part number, a 2-contact block slow break, discontinued in 2000 and replaced by the current XCSPL offer in 2017, having a 2-contact block slow break too.

Was this helpful?
What can we do to improve the information ?