Technical FAQs

Ask a Question

Does the ION7650 and ION7550 use the same Firmware file for V374 and V401?

Issue
Previous Firmware releases before V373 had separate Firmware files for the ION7650 and ION7550.

Product Line
ION7650/7550

Environment
Firmware

Resolution
For Firmware V374 and V401 there is a single file that works for both the ION7650 and ION7550.

For more information on this update see What's new in PowerLogic ION7550/ION7650 firmware version 374 & 401.
Was this helpful?
What can we do to improve the information ?