Technical FAQs

Ask a Question

Preventa XCS - Dimensions of the obsolete XCSTL5/7 having 5 digits in the part number, discontinued in 2000

Hereafter the dimensions (in mm) of the obsolete XCSTL5/7 switch having 5 digits in the part number, a 2 contact block slow break, discontinued in 2000 and replaced by the current XCSTL offer in 2017 having a 3-contact block slow break.

   
Was this helpful?
What can we do to improve the information ?