Technical FAQs

Ask a Question

Osisense XT - Cross-reference of the XUZB32 fixing clamp

The XUZB32 fixing clamp is discontinued since 2010. It is not replaced for the following reason. It was a fixing accessory for the obsolete XT1 & XT4 capacitive sensors discontinued in 2008. The current XT1 & XT2 capacitive sensors are supplied with their own brackets. Alternative could be the 90° metallic bracket XXZ30 for example.

Was this helpful?
What can we do to improve the information ?