Technical FAQs

Ask a Question

Release Notes for CitectSCADA 2015 Service Pack 1

Issue
The CitectSCADA 2015 Service Pack 1 includes several product updates and enhancements, providing improvements in stability, performance and functionality.

PowerSCADA (PSE) 8.1 Service Pack 1 (uses the same release notes) was created as a special case to fix a customer issue and thus was never officially released for general public use. It allows PSE to use Citect patches.  In general it is a “Power-Build” version of Citect 750 Service Pack 1 created by Citect to serve the PSE specific customer. 

Product Line
PowerSCADA Expert 8.1 (CitectSCADA 7.5)

Environment
Service Pack

Cause
Incorporating new or modified features.

Resolution
The attached Release Notes for Service Pack 1 discusses the following topics:
  • What’s New in CitectSCADA 2015 SP1
  • Service Pack Installation
  • Service Pack Uninstall
  • Files changed in this Service Pack
  • Known Issues
  • Issues resolved in this Service Pack
Was this helpful?
What can we do to improve the information ?