Technical FAQs

Ask a Question

Osisense XC - XCKM215 or XCKM215H29 limit switch cross-reference

The XCKM215 or XCKM215H29 limit switch has been completely discontinued in november 2003 (obsolete contact version). It was in fact an XCKM115(H29) switch with some contact state indicator; see attached picture. It used the ZCKM2(H29) special contact body. It is replaced by the XCKM115 or XCKM115H29 since 2004, having a new contact block.

       
Was this helpful?
What can we do to improve the information ?