Technical FAQs

Ask a Question

Osisense XC - Equivalent of the XCKJ20543H7 limit switch

The XCKJ20543H7 limit switch reference is no more available in 2017 as a complete limit switch. It has to be ordered by the sub-assemblies ZCKJ2H7 body + ZCKE05 rotary head + ZCKY43 variable length steel roller lever. Note that the XCKJ20541H7 complete switch is available to order in 2017 (picture attached - difference roller material).

Was this helpful?
What can we do to improve the information ?