Technical FAQs

Ask a Question

HTTP Error 500.24 when trying to access the Rate Editor in PME 8.1

Issue
 Rate editor produces the following error : An ASP.NET setting has been detected that does not apply in Integrated managed pipeline mode
 
Product Line
PME 8.1 Rate Editor

Enviroment
Internet Information Services (IIS)
 
Resolution
The ASP.NET impersonation is enabled and it must be disabled for the Rate editor to work. To disable this feature:
 
1- Start Internet Information Services (IIS) from administrative tools.
2- Navigate to the RateEditor site by expanding site tree and the default site tree thereafter. 
3- Double click on authentication option as shown below.

4- Disable the ASP.NET Impersonation by highlighting the option and then click disable on the action panel.
5- Restart IIS by typing the following command in command prompt(cmd): IISreset.
 

 

Was this helpful?
What can we do to improve the information ?