Browse FAQs

What version of firmware is required in Lexium 05 to support CANMotion (CANsync) ?

Published date: 23 October 2018

CANMotion support, as in with LMC20 motion controller, in Lexium05 was implemented at firmware version 1.201 and newer.
Therefore, any Lexium 05 connected to CANMotion must have firmware level greater than 1.201.  
For example, firmware version 1.125 will not operate on CANMotion bus.  The drive will not respond to commands.

Users of Lexium 05 on CANMotion are advised to flash the firmware to the most updated version, which is version 1.502 


rev 10-23-18

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.