Browse FAQs

How to add the USB Barcode Scanner to HMIG5U in Vijeo Designer

Published date: 20 March 2019

Issue:
How to add the USB Barcode Scanner to HMIG5U in Vijeo Designer

Product Line:
Vijeo Designer, HMIG5U, HMIG5U2

Resolution:
The USB barcode scanner does not need to be added in Vijeo Designer as Windows will treat a USB barcode scanner as a keyboard. When it scans, Windows will take the input and type it as if a user was typing on a keyboard. The catch is the cursor must be enabled before the scan is made in the Vijeo Designer Runtime.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.