Browse FAQs

What is the part number for the power connector for the HMIPEP series?

Published date: 20 March 2019

Issue:
What is the part number for the power connector for the HMIPEP series?

Product Line:
HMIPEP series

Resolution:
The part number for the power connector to the HMIPEP series is the HMIYEM1211.

This part number comes in a package of 5 which can be used to wire up the Ethernet, COMs, and USB port.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.