Technical FAQs

Ask a Question

Osisence XM - UL and C-UL-US certificates of the XMEP pressure transmitters for mobile equipment

1) Here UL QUYX.E356157 certificate link, concerning the XMEP pressure transmitters for mobile equipment
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=QUYX.E356157&ccnshorttitle=Process+Control+EQUIPMENT,+Electrical&objid=1082525948&cfgid=1073741824&version=versionless&parent_id=1073992554&sequence=1

2) The C-UL-US Classification Mark on the XPEM sensor indicates compliance with both Canadian and U.S. requirements. Below UL certificate including the Canadian one (C-UL-US label) : QUYX7.E356157 .... Certified for Canada
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=QUYX7.E356157&ccnshorttitle=Process+Control+EQUIPMENT,+Electrical+Certified+for+Canada&objid=1082632892&cfgid=1073741824&version=versionless&parent_id=1073992557&sequence=1
Was this helpful?
What can we do to improve the information ?