Technical FAQs

Ask a Question

Osisense XC - How to order the complete switch "XCKJ18511H29"

The complete switch XCKJ18511H29 does not exist in the commercial data base, you have to order the following sub-assemblies and assemble them to get it : ZCKJ18H29 contact body (gold flashed contacts of the ZCKJ1H29) + ZCKE05 rotary head + ZCKY11 roller lever.
Was this helpful?
What can we do to improve the information ?