Technical FAQs

Ask a Question

M340 firmware version 2.9

Title
M340 firmware version 2.9
 
Issue
M340 firmware version 2.9
 
Product Line
M340
 
Environment
Vendor, Product, Version
 
Cause
N/A
 
Resolution
 Attached is the M340 firmware version 2.9 release notes of issues that were resolved.
 
Was this helpful?
What can we do to improve the information ?