Technical FAQs

Ask a Question

Are the Magelis iDisplays rated for Class1 Div2?

Issue:
Are the Magelis iDisplays rated for Class1 Div2?

Product Line:
Magelis, Class1 Division2, HMIDID64DTD1, HMIDID73DTD1

Resolution:
Yes, the Magelis iDisplays are rated for Class1 Div2.
Was this helpful?
What can we do to improve the information ?