Technical FAQs

Ask a Question

What options are available to have the M580 communicate to Momentum DIO base?

Issue:
What options are available to have the M580 communicate to Momentum DIO base?

Product Line:
distributed I/O

Environment:


Cause:


Resolution:
M580 will communication to the 170ENTxxxxx ethernet tophats.  But if the DIO are on an Interbus tophats, then the tophats needs to be replaced with to the 170ENT11001 or 170ENT11002 tophat.  
Was this helpful?
What can we do to improve the information ?