Technical FAQs

Ask a Question

HMIGTO targets only have one USB A port. Is it possible to connect both USB barcode scanner and a USB flash drive at the same time?

Issue:
HMIGTO targets only have one USB A port.  Is it possible to connect both USB barcode scanner and a USB flash drive at the same time?

Product Line:


Environment:


Cause:


Resolution:
In order to connect the USB barcode and flash drive onto the HMIGTO by using a USB hub.  Make sure that the USB hub has an external power input.
Was this helpful?
What can we do to improve the information ?