Technical FAQs

Ask a Question

Application Configuration Utility is Not Functional After it is Opened

Issue
After opening Application Configuration Utility, the utility is not responsive and it is trying to determine the service status unsuccessfully:



Product Line
PowerSCADA Expert 8.0, 8.1 (PSE 8.0, 8.1)

Environment
Windows OS
Windows Services

Cause
The problem could occur when the user is connecting through a VPN or an antivirus software is installed on the server.

Resolution
In this case the user was accessing the PowerSCADA server through VPN and an antivirus software had the firewall enabled.

1.  Disable the firewall (click on 'Firewall - on' to toggle it):




2.  Close and reopen Application Configuration Utility:


 
Was this helpful?
What can we do to improve the information ?