Browse FAQs

How do we enable/disable the Front USB port on the HMIGTU series.

Published date: 14 February 2019

Issue:
How do we enable/disable the Front USB port on the HMIGTU series.

Product Line:
HMIGTU Series

Resolution:
Enabling the Front USB Ports

To enable the front USB ports for the Premium Box (HMIG3U):

1. In the Target's Hardware properties, define the Front USB Ports on Display properties. Set the USB Port (Host) and Mini USB Port (Device) properties to Enabled. 

2. In the Target's General properties, make sure the Preserve Run-Time Data property is not selected. If the property is selected, the target settings in build time will overwrite the target machine settings in runtime. 

3. Download the project to the target machine, and start run time. 

To enable the front USB ports for the Open Box (HMIG5U/HMIG5U2):

1. In Windows, go to Control Panel. Select Hardware and Sound.

2. On the Hardware and Sound page, select Front USB Settings. The Front USB Settings dialog opens.

3. Select Enable. Click OK and restart Windows to apply the change.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.