Technical FAQs

Ask a Question

AS-B872-001 specifications and wiring diagram

The attached pdf is also applicable to the *AS-B872-002 as well as the *AS-B872-001.



**Note: The 800 series family of  I/O is obsolete. Please consider alternatives offered in the Quantum or BMX families of IO .
Was this helpful?
What can we do to improve the information ?