Technical FAQs

Ask a Question

PM5000 Series Device Simulator

Issue
User may want to experience PM5000 Series meter without a physical device around. The user needs to learn the display features of the PM5000 Series Meter. 

Product Line
PM5000 Series Meter

Environment
Device Simulation

Cause
It may be desired to experience the device and its functions without the physical device in-hand.

Resolution

Download the following attachment to simulate PM5000 Series Meter
This simulator provides the user with the ability to navigate through the display and observe what is capable through the front display (setup, monitoring, and security)
 
Was this helpful?
What can we do to improve the information ?