Browse FAQs

Is the Telefast ABE7CPA31 internally fused? If so, are they replaceable?

Published date: 11 February 2019

Issue:
Are there fuses on the Telefast ABE7CPA31 that can be replaced by end users? 

Product Line:
Telefast, Modicon Premium, Modicon X80

Resolution:
 The ABE7CPA31 does not have any internal field replaceable fusing.  Any desired fusing must to be done externally. There is a 25mA current limiter on each channel for protection. The current limiter will trip and reset. They are not field replaceable.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.