Technical FAQs

Ask a Question

Why am I getting the error: Seek failed. Communication method, when trying to upload recipes from the Magelis HMI?

Issue:
Why am I getting the error: Seek failed. Communication  method, when trying to upload recipes from the Magelis HMI?

Product Line:
Vijeo Designer, Magelis

Environment:


Cause:


Resolution:
This issue usually occurs when the version of Vijeo Designer buildtime is higher than what is in the Magelis Runtime.  First, determine the version of the runtime that is in the Magelis.  Then install that version of Vijeo Designer buildtime.  Then use that version of Vijeo Designer to upload recipes from the Magelis.  
 
Was this helpful?
What can we do to improve the information ?