Technical FAQs

Ask a Question

CM4000 Download Incomplete when making changes to Onboard Alarms/Events in ION Setup v3.0

Issue
When making a change to the onboard alarms/events section of any CM4000 in ION Setup when it is sent to the meter the software returns Download Incomplete. 

Product Line

ION Setup v3.0
CM4000

Environment
ION Setup v3.0 with CM4000' Series Meters

Cause
Due to the variations in firmware the meter responded differently back to ION Setup. 

Resolution
Build 17033 and greater should resolve this issue. 
Upgrade to the latest ION Setup v3.0 by downloading it HERE
 
Was this helpful?
What can we do to improve the information ?