Technical FAQs

Ask a Question

PowerSCADA Expert compile fails with Fatal error Cannot read from file variable.sqx or remap.dbf

Issue
While trying to compile the project an error occurs "Cannot read from file variable.sqx" or "Cannot read from file remap.dbf"

Product
PowerSCADA Expert (PSE) 7.4

Environment
Incremental compile is enabled

Resolution
Uncheck incremental compile.

In Citect Project Editor go to Tools -> Options. (Uncheck "Incremental compile")

Was this helpful?
What can we do to improve the information ?