Technical FAQs

Ask a Question

Is the EM4200 series meter supported with the Sub Meter Display (SMD) or SMDOPN?

Issue
Is the EM4200 series meter supported with the Sub Meter Display SMD or SMDOPN?

Product Line 
EM4200 series meters 

Cause
User would like to display values from EM4200 meter locally on Sub meter display (SMD) or SMDOPN. 

Environment 
Displaying values from EM4200 series meter on display. 

Resolution
Initially, the SMD or SMDOPN was not supported with the EM4200. 

However, a release of new firmware for the SMD allows EM4200 support. The latest firmware version (v29) for the SMD will provide functionality to see the values from the EM4200 series meters.
Note: v29 firmware can be found attached to this article along with the the step-by-step procedure for upgrading the SMD using DLF-3000. 

The DLF-3000 utility can be downloaded using the following link:
DLF300 Download
Was this helpful?
What can we do to improve the information ?