Technical FAQs

Ask a Question

Osisense XM - CAD 3D files of the XMEP pressure sensors

Hereafter telemecanique Sensors@ providing 3D CAD files of XMEP pressure sensors (link with Traceparts library). XMEP = X Mobile Equipment Product, is dedicated for mobile equipment like agricultural tractors, aerial platform on trucks, garbage trucks, construction vehicule, harbor telehandler ...
http://www.tracepartsonline.net/(S(qvyvcr32jhd2ihhydmney3dz))/content.aspx?ClsID=/F_TELEMECANIQUE_SENSORS/TELEMECANIQUE_SENSORS.010/TELEMECANIQUE_SENSORS.010.020/TELEMECANIQUE_SENSORS.010.020.010/TELEMECANIQUE_SENSORS.010.020.010010/&tp=2&st=0&Lang=en&Class=TELEMECANIQUE_SENSORS&fwsid=TELEMECANIQUE_SENSORS&ttl=Type+XMEP+%c3%9826+X+61mm
Was this helpful?
What can we do to improve the information ?