Technical FAQs

Ask a Question

What is the BMECRA312x0 DDT parameter MAX_PACKET_INTERVAL?

Title
BMECRA312x0 DDT parameter MAX_PACKET_INTERVAL
 
Issue
BMECRA312x0 DDT parameter MAX_PACKET_INTERVAL
 
Product Line
M580
 
Environment
Unity Pr0 11.1
 
Cause
N/A
 
Resolution
 In BMECRA312x0 DDT the parameter that is called, MAX_PACKET_INTERVAL tells you the maximum packet interval (ms) for output packets from the M580 scanner to the CRA drop,

 
Was this helpful?
What can we do to improve the information ?