Browse FAQs

Which driver should be used for the Model 98A in SPM and PME?

Published date: 01 February 2019

Issue
Schneider Electric has 2 temperature controllers:
Model 98 - Black face plate.
Model 98A - Green and white face plate (newer model) 

Which driver is required to communicate to the Model 98A. Can the same driver used for the Model 98 be used for the Model 98A?

Product Line
Model 98
Model 98A
ION Enterprise
StruxureWare Power Monitoring (SPM)
Power Monitoring Expert (PME)

Environment
Management Console
Driver

Resolution
The Model 98A uses the same driver as the Model 98. Please reference the below links for the Model 98 driver.

SPM 7.x and ION 6.0 Model 98 driver
PME 8.0 and PME 8.1 Model 98/98A driver
PME 8.2 and PME 9.0 Model 98/98A driver
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.