Technical FAQs

Ask a Question

What is the replacement for ATV71 drives?

Issue:
What will replace the ATV71 series drives?

Product Line:
ATV71 series drives.

Environment:
Replacement drive
 
Cause:
n/a

Resolution:
Generally the ATV930 series will be a good replacement for the ATV71 series but the application should be evaluated before ordering to be ceratin.  Based on the application, another drive may be a better choice, it should be evaluated on a case by case basis.

 
Was this helpful?
What can we do to improve the information ?