Technical FAQs

Ask a Question

Is the Unity Pro 11.1 iso file compatible with the Windows 10 Mount utility?

No, the Unity Pro 11.1 iso file is not compatible with the Windows 10 mount utility. You can use DVDFab Virtual Drive for windows 10 to mount the iso file.
Was this helpful?
What can we do to improve the information ?