Browse FAQs

Can I update the M241 application with an SD card when the user management is enable?

Published date: 16 August 2019

If the user management is enabled, it is not possible to update the application via SD card. The script which is on the SD card is blocked by the user management and will not be executed successful.
 
To update an application with user management enable, it is necessary to connect with SoMachine or at least with the Controller Assistant (manage image to change the application) to the controller.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.