Technical FAQs

Ask a Question

Where do I insert the battery in a M221 controller?

The M221 battery is inserted at the top of the PLC as shown the in attached picture.

You also need the battery holder that is included with the M221.

User-added image

Was this helpful?
What can we do to improve the information ?