Technical FAQs

Ask a Question

What is the maximum permitted distance between the 140ARI03010 and the sensor?

When using 3 or 4 wire RTD's the maximum distance between the module and the sensor is 200 meters.
If you're using 2 wie RTD's the distance is limited only by the user defined accuracy of the application.
Was this helpful?
What can we do to improve the information ?