Technical FAQs

Ask a Question

Osisense XS - Data sheet of the old proximity sensor XSDJ60733

The old proximity sensor XSDJ60733 has changed reference to XSDJ607339 before 1985. The last digit 9 means "non flush mountable". Attached the XSDJ607339 data sheet, valid to the old XSDJ60733 part number. Difference between XSDJ60733 and XSDJ607339, the first reference has a fixed body, the new one has a plug-in body. Attached dimensions (in mm) of the old XSDJ60733 sensor. Fixing distances are the same for both references.

Was this helpful?
What can we do to improve the information ?