Technical FAQs

Ask a Question

A Scada Project is not Listed in One Line Configuration Utility Drop Down List

Issue
A user created a new PSE project with oneline and breaker animation.  After opening One Line Configuration utility, the project would not show up in the drop down list of projects.

Product Line
PowerScada Expert 8.1 (PSE 8.1)

Environment
One Line Configuration Utility

Cause
Standard norms were not followed when creating the project.

Resolution
PLS_Include was not one of the included projects.  After including it to the list of included projects, the project name appeared in One Line Configuration utility's drop down list.
 
Was this helpful?
What can we do to improve the information ?