Technical FAQs

Ask a Question

Osisense XC - Can antenna ZBRA1 be used in conjunction with the XZBWE112A24 wireless transmitter for one sensor

The optional ZBRA1 antenna is not compatible with the wireless transmitter XZBWE112A24. It is only compatible with the XCKW1* wireless & batteryless limit switches. Attached XCKW* catalogue extract showing this association. The XZBWE112A24 wireless transmitter for one sensor is used in conjunction with the XZBWR2STT24 receiver for 2 transmitters.

Was this helpful?
What can we do to improve the information ?