When I click on the "Data Selection" ellipses Unity appears to freeze or lock up. How do I correct this condition?
This condition is most often observed after using Unity with an extended monitor. If Unity is closed while it's on the extended monitor, and the monitor is removed,
Unity will continue to operate as if the the extended monitor were still connected. In effect part of the Unity application is still on the extended monitor and you need
to drag it back to your local display on the PC.
Using your keyboard.. Select ATL Space M
Use the left arrow key on your keyboard to bring the Unity Data Selection window back into view.