Technical FAQs

Ask a Question

Preventa XY2C - Data sheet of the adapted XY2CH14250TK rope pull switch in TK protective threatment and low temperatures

Find attached the data sheet of the adapted XY2CH14250TK rope pull switch in TK protective threatment, available to order in 2017 (not in stock). The TK special threatment corresponds to products able to resist to corrosive environmental conditions (harsh industrial environment). For this rope pull switch, a special TK blue painting instead of the standard red one and cover screws in stainless steel are used. Note that the cover is in stainless steal in the standard red XY2CH switches. In january 2017, the XY2CH14250 using silicone below & cap, is not available to order. Such references having silicone below and cap on the reset booted button, can be used in low temperatures down to -40°C in operation.
Was this helpful?
What can we do to improve the information ?