Browse FAQs

Osisense XC - What is the UL94 flame classification of the blue XCKW1 plastic case?

Published date: 03 July 2019

The plastic case of the blue XCKW1 wireless & batteryless limit switches is a blue Valox 553, or PBT+PC GF30. It is flame classified UL94 V-0. PBT stands for polybutylene terephthalate, PC for polycarbonate, GF30 means 30% glass fiber reinforced.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.