Technical FAQs

Ask a Question

Osisense XC - Picture of the red limit switch XCLJ50511H29

Attached picture of the red limit switch XCLJ50511H29 composed of 2 red painted sub-assemblies ZCKJ5H29 body + ZCKE05 head & the roller lever ZCKY11. Logistic situation in 2017 available to order.  XCLJ50511 reference does not exist. Complete switch reference is indicated on the red body.

Was this helpful?
What can we do to improve the information ?