Technical FAQs

Ask a Question

What causes the Magelis iPC HMIBM Modular Box to abruptly shutting down?

Issue:


Product Line:
What causes the Magelis iPC HMIBM Modular Box to abruptly shutting down?

Environment:
HMIBM Modular Box

Cause:


Resolution:
This is a known issue where the BIOS setting for CPU shutdown temperature is set too low.  Follow the instructions below to change the temperature settings.
1.    Press “Delete” key enter BIOS when system boot up.
2.    Select Advanced Tab -> iManager Configuration
3.    CPU Shutdown Temperature  Change to 105° C
4.    Select Save & Exit -> Save Changes and Exit
Was this helpful?
What can we do to improve the information ?