Technical FAQs

Ask a Question

Preventa XCS - Update instruction sheet of the special XCS74* safety switch with a mushroom pushbutton at the back of the enclosure

Find attached the 2017 instruction sheet of the special safety switches XCSE74* with locking function having an unlocking mushroom pushbutton at the back of the product in addition. Concerned complete references : XCSE7411, XCSE7412, XCSE741214, XCSE7431. Such references are not listed in the Preventa XCS catalogue. Because of the obsolescence of the red mushroom, it is replaced by a black mushroom (same diameter).

Was this helpful?
What can we do to improve the information ?