Technical FAQs

Ask a Question

Launched Runtime on the Magelis HMIPSP and getting error "incorrect reference".  What causes this error?

Issue:
Launched Runtime on the Magelis HMIPSP and getting error "incorrect reference".  What causes this error?

Product Line:
VJDSNRTMPC, HMIPSP

Environment:


Cause:


Resolution:
The Vijeo Designer Runtime did not support the Magelis HMIPSP targets until Vijeo Designer v6.2 SP4.1.  Please install SP4.1 or higher to support HMIPSP.
Was this helpful?
What can we do to improve the information ?