Technical FAQs

Ask a Question

What is the replacement for the Magelis Smart iPC 8.4" MPCST11NAJ00T?

The MPCST11NAJ00T, Smart 8"4, AC is replaced by the (HMIPWC5D0E01) 10” DC touch screen.  The enclosure cut-out are different but the screen resolution are the same in Vijeo Designer.

Power supply:
ABL8RPS24050 (100~500VAC...24VDC/5A)
or
ABL4RSM24050 (120~230VAC...24VDC/5A).
Was this helpful?
What can we do to improve the information ?