Technical FAQs

Ask a Question

Does the Device Simulation work when the task bar is on the left of the Screen?

Goals and Symptoms       
Some customers have a PC with the task bar on the left of the screen. They complain that the device simulation window of Vijeo Designer is displayed outside the screen. In this case, it is impossible to see the simulation window and to move it inside the screen.
  
Causes and Fixes       
 
The Device simulation tool does not work when the task bar is on the left of the screen. You have to move the task bar on the bottom of the screen.
Even if the task bar is moved on the bottom of the screen, the device simulation window keeps the last position which is outside the screen. You have to follow the steps provided in the video file in order to be able to display the Device Simulation window inside the screen.
 
Was this helpful?
What can we do to improve the information ?